Parameter Library Examples

The VisualApplets example designs in this chapter demonstrate how to use and manipulate parameters. All examples can be found in the VisualApplets installation directory in sub-directory examples i.e. “%VASINSTALLDIR%/examples/AdvancedVAFunctions/Parameters Library”.

A detailed introduction into library Parameters you find in the Operator Reference, section Library Parameters.

The following sections show an overview on all examples. A brief introduction is presented as well as the folder and filename. All examples use a default hardware platform. Nearly most of them can easily be converted to other hardware platforms. See 'Target Hardware Porting' for more information on how to switch the hardware platform.